This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM66100: Can pin6 handle the 12V?

Part Number: LM66100

Team,

My customer is switching between two voltages. For one he uses the LM66100 and the other having to use a diode.  The voltages are 5 and 12V.

Question - when the 5V is off and 12V is on, will the LM66100's out pin6 handle the 12V? 

Thanks

Viktorija