Part Number: TPS25947
Hello expert,
I have question for TPS25947's Itimer and Ilim.
First, can I configure Itimer as longer than 30ms?
Also could you provide recommended capacitor value for achieving 30ms Itimer including variation from TPS25947?
Second, could I configure Ilim lower than 0.5A?
Datasheet said this device can be configure Ilim as 0.5A~6A with 10% accuracy.
I though it mean that this device can be configure Ilim as lower than 0.5A but cannot guaranty accuracy.
Is it correct?
I understood it is difficult to provide accuracy for Ilim lower than 0.5A setting but could you provide accuracy information for Ilim lower than 0.5A as just information?
I'm looking forward to hearing back from you.
Best regards,
Kazuki Kuramcohi