Hi,
I wrote this program to pilot led1, led2, led3 and a group of led (namely kbd). I modify control flow by writing local variables (ra, 42h to 44h) for each engine and global variables (rd, 3eh)
Instruction on all 3 engines are almost identical but only engine 1 seems to work. All three engines are configured to run in mode 'free run' and my startup configuration works very well with other programs that use all three engines but this particular program don't.
Maybe I'm missing something?
Thanks for your support,
Best regards,
Daniel
_____________________________
led1: dw 0000000000000001b led2: dw 0000000000000010b led3: dw 0000000000000100b kbd: dw 0000000111111000b all: dw 0000000111111111b .segment program1 ; LED 1 and KBD Program map_addr all set_pwm 0 m1: map_addr kbd set_pwm rd map_addr led1 ld rb, 0 je rb, ra, l1off ld rb, 1 je rb, ra, l1pulse ld rb, 2 je rb, ra, l1flash ld rb, 3 je rb, ra, l1on l1off: set_pwm 0 branch 0, m1 l1pulse: ramp 0.5, 255 ramp 0.5, -255 branch 0, m1 l1flash: set_pwm 255 wait 0.3 set_pwm 0 wait 0.3 branch 0, m1 l1on: set_pwm 255 branch 0, m1 end .segment program2 ; LED 2 Program m2: map_addr led2 ld rb, 0 je rb, ra, l2off ld rb, 1 je rb, ra, l2pulse ld rb, 2 je rb, ra, l2flash ld rb, 3 je rb, ra, l2on l2off: set_pwm 0 branch 0, m2 l2pulse: ramp 0.5, 255 ramp 0.5, -255 branch 0, m2 l2flash: set_pwm 255 wait 0.3 set_pwm 0 wait 0.3 branch 0, m2 l2on: set_pwm 255 branch 0, m2 end .segment program3 ; LED 3 Program m3: map_addr led3 ld rb, 0 je rb, ra, l3off ld rb, 1 je rb, ra, l3pulse ld rb, 2 je rb, ra, l3flash ld rb, 3 je rb, ra, l3on l3off: set_pwm 0 branch 0, m3 l3pulse: ramp 0.5, 255 ramp 0.5, -255 branch 0, m3 l3flash: set_pwm 255 wait 0.3 set_pwm 0 wait 0.3 branch 0, m3 l3on: set_pwm 255 branch 0, m3 end