Other Parts Discussed in Thread: BQ24075, TPS63060,
Hi,
I am new to electronics design and i am confused in selecting the proper regulator,please help.
I designed a schematic using BQ24075 to power device running on battery(3.7 nominal voltage) and first i selected AMS1117 as regulator but it is not working and i realised due to drop out voltage OF AMS1117-3.3 it requires minimum 4.4 to operate.
Can i use TPS63070/TPS63060 to regulate voltage coming from battery to get regulated 3.3V and i require only max. Of 1A current for my application and current rating of both TPS63060/TPS63070 ics is much higer than 1A.
Is it a good solution to use TPS63060/TPS63070 because current ratings are high.
If it is good to use which one should i go for TPS63060/TPS63070?
If both are not good which IC should i select.
My requirements are vout =3.3V ,iout = 1A and iq have to be as low as possible for powering the whole device
Thanks and regards,
P.Akhil.