Dear team,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear team,
Hi Urs,
Per datasheet section 7.3 on page 6, the maximum RMS discharge current is 5A with peak discharge current for 1us of 9A.
Per datasheet section 8.3.11.1.4, The charger device continually monitors and compares VBUS to VSYS to protect against a system short-circuit event. In the event that VSYS drops to within 250 mV of VBUS during operation, a short circuit event is flagged and the converter stops switching. The SYS_SHORT_FLAG or SNS_SHORT_FLAG bit is set and an INT pulse is asserted to the host. The device attempts to recover from this condition automatically.
Regards,
Jeff
Hi Jeff,
Hi Urs,
Per datasheet section 8.3.13.2 Battery Over-Discharge Protection, when the battery is discharged below VBAT_SHORT_HYS, the BATFET is turned off to protect battery from overdischarge.To recover from over-discharge, an input source is required at VBUS. When an input source is plugged in, the BATFET turns on. The battery is charged with IBAT_SHORT current when the VBAT < VBAT_SHORT, or pre-charge current as set in IPRECHG registers when the battery voltage is between VBAT_SHORT and VBAT_LOWV.
Regards,
Jeff