Dear
LM5176 can not take up the load, power supply full power is 450 w, is currently in 2 groups of 225 w LM5176 IC control circuit of the parallel test, the output voltage is 12 v, below 19 v can bring full, but aging for A few minutes MOS tube and IC after the temperature rise to about 60 ℃ or so off voltage will happen until the protection, pick up the load model is to use electronic load CC model test with 37.5 A
any advive? thanks in advance