This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62172: TPS62172 - ESD diode rating

Part Number: TPS62172


Hello Team,

the voltage rating for the Enable pin shows that the pin has the ESD diodes.

To increase system robustness there is the need to protect the pin further. 

To achieve that, the plan would be to limit the current with a resistor in case of any voltage. (no additional TVS, zener diodes)

This would be for a failure scenario and not a typical use/stress the part will be subject to.

Thus the question, what is the typical (end even better the max) current value, the TPS62172 ESD diodes can withstand.

If needed, I have the NDA in place.

Thanks,

SunSet