Hi Sir/madam
My charger should operate in the following conditions
input voltage : 15V
input current :2.4A
output voltage:12V
output current : 1.2A
my charger is working without system in the sense it should charge only the battery...
what are the registers i should set so that it would give exact output please help me with these i have tried different boards and burnt 7 IC please reply to this thread.....
thank you in advance.......