This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8860-Q1: About the accuracy of the current value

Part Number: LP8860-Q1

Hi,

I would like to ask you about the accuracy of the current value of LP8860-Q1.
I have set DRV_LED_CURRENT_SCALE [2: 0] to "101" to set the LED current to 100mA.
Moreover, RISET = 24kΩ ± 1% is used.
(Question)
What is the current accuracy for the above settings?
Is it ± 4%, which is the sum of the accuracy of the device itself (± 3%) and the accuracy of the resistance value (± 1%)?
Looking at the thread below, the current accuracy is only guaranteed at 150mA.
Also, if I set it to 100mA and it's not guaranteed, why?

Best regards,

e2e.ti.com/.../627590

  • Hi Kaji,

    If you compare the output current to the  ideal value of current equation with 24 kohm, the accuracy will be the root mean square value of all the errors.

  • Thank you for your reply.
    I will change the content of the question and I will ask you again.
    A thread posted in the past states that ± 3% accuracy is guaranteed only at MAX 150mA.
    It is also stated that the accuracy deteriorates as the current value setting is lowered.
    I would like to know if the accuracy of ± 3% is guaranteed when DRV_LED_CURRENT_SCALE [2: 0] is set to 100mA of "101".
    Is it possible to answer my question?

    Best regards,

  • Hi Sir,

    The accuracy of current is related to the characteristic and accuracy of internal circuit. Therefore,  if you set it to 100mA and it's not guaranteed.