Hi TI,
According to LM3881 data sheet, Cadj of 10nF will make delay between FLAG2 and FLAG1 to be about 10ms.
What's the max delay can be set?
If I put Cadj as 20nF, does it mean that the delay becomes ~ 20ms?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI,
According to LM3881 data sheet, Cadj of 10nF will make delay between FLAG2 and FLAG1 to be about 10ms.
What's the max delay can be set?
If I put Cadj as 20nF, does it mean that the delay becomes ~ 20ms?
Thanks.
I've got the same question.
Are there any limitation on the maximum and minimum of Cadj?
Hello
The capacitor timing clock is about 120ns/nF. so 10nF is about 1.2ms per clock. The delay is about 8-9 clock between each flags which is about 10ms.
For 20nF capacitor the clock period is about 2.4ms. The delay is about 8-9 clock between flags which is about 20ms-21ms.
Regards
Yihe