This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25710: Simpler part comparing BQ25710 suggestion

Part Number: BQ25710
Other Parts Discussed in Thread: BQ25619

Hi Team,

Could you help to find simpler part comparing BQ25710?

 

Spec:

power path (can support adapter/battery swtich)

I2C(SMBUS) can report voltage..etc to MCU

Vout:3.3V

Vbattery:3.7-4.2V

Vin:5V

Many Thanks

Jimmy

System may ~1A

  • Hi Jimmy,

    We have several 1S chargers which you can search at the link below.  I recommend starting with BQ25619, if system load and charge current are < 1.5A.  Keep in mind that Vout=3.3V is not possible with any of our power path chargers as the SYS/OUT output follows the battery up to 4.2V.

    www.ti.com/.../products.html Buck&p2192=Power Path

    Regards,

    Jeff