This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS26630-33EVM: No Connect NC PINs routed on Eval Board

Part Number: TPS26630-33EVM

Hello,

I am wondering why in the TPS26630-33EVM two of the No Connect (NC) PINs are being used. PIN#19 with VOUT and PIN#24 with VIN1?

The other NC PINs are all connected to GND.

  • Hi Jawad,

    Welcome to E2E!

    Pins 19 to 24 are N.C pins. These are internally not connected and are floating pins. These can be connected to the nearest planes (VIN ,VOUT or GND). For example, pin 24 can be connected to VIN and pin 19 can be connected to VOUT in layout to get wider traces in order to minimize the PCB trace impedance.

    Best Regards, Rakesh