Hi,
My customer would like to know if there is a single channel version of the TPS2561A?
They really like two features of the 2561A that make it attractive for their application. First the device has a soft current limit (i.e. continues providing power at Ilim instead of shutting down). Second, the output current limit is adjustable in the 250ma to >1.5A range. However, the device has two independent channels and our application only needs a single one.
Thanks,
Soumya