Other Parts Discussed in Thread: BQ25601
Hi,
I am using a bq27z561 gauge IC for monitoring the battery. In few instances we have observed that the battery capacity reaches only up to 96% when charging the battery from completely discharged state. However if we reset the fuel gauge using software command, then the capacity corrects itself and reaches 100%
In normal case where we charge the battery from 20-30%, the capacity reaches 100% every time.
Need help in understanding which parameter is incorrectly set in fuel gauge that is causing this issue