This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28Z610-R1: Update Status unchanged (0x04->0x05)

Part Number: BQ28Z610-R1

Hi, Ti team

1S2P BAT INR18650-35E / Samsung (Chem ID : 2361)

- Capacity : 3400mAh (2P : 6800mAh)

- nominal Voltage : 3600mV

 

After checking the sula777 and running Cycle in order, Update Status did not change after full charge. (0x04 -> 0x05)
When we checked the DOD, we found that it was measured around 6470 (95%).

 

- Chem ID selection : 2361 (Confirmed by I2C: 06 00 61 23)

- DA configuration : CC0 Low

- Design capacity : 2448cWh

- Taper Current : 100mA

- Term Voltage : 3000mV

- Chg current Threshold : 64mA

- Dsg current Threshold : 57mA

- Quit current Threshold : 14mA

 

Is there something I missed? I attached the log and gg file, so please check it.

201125.zip

thanks.

huh.