This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR50410-Q1: Maximum Input current limit

Genius 9880 points
Part Number: LMR50410-Q1

Hi Team, 

Good day, can you please confirm what is the Maximum Input current limit of LMR50410-Q1. The customer plans to use it as converter from 28V solar panel to a 5V output to power sensing circuit. 

Thank you and looking forward for your kind response.

Regards,

Maynard

  • Hello Maynard,

    TI does not specify a Maximum input current limit for this device, however the High-side current limit (ISC) specified in the Electrical Characteristics table does specify the amount of current through the high side MOSFET that will cause the device over current protection feature to be tripped. (1.6A typical)

    This essentially serves as the maximum allowed input current to the device.

    Regards,

    Harrison Overturf