Part Number: TPS22976
Other Parts Discussed in Thread: TPS25982
Dera sir
1.When TPS22976 is applied to VIN capacitor <VOUT capacitor, do I need to worry about damage to TPS22976?
VIN capacito(88uF~120uF) < VOUT capacitor(200u~470u)
2.Do I need to follow the datasheet Reverse Current Blocking Figure 10-4 in the application where the IN capacitance is less than the OUT capacitance to avoid current passing through the body diode to damage the TPS22976?
3.Is there a Thermal Shutdown Plot During Start-up Figure available for TPS22976? Such as TPS25982 datasheet Figure 53