This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2121: switching between IN_1 and IN_2 issue

Part Number: TPS2121

We prepared a design using TPS2121, for a reference part of the design attached here. So please review our schematic design and suggest if any changes required. 

We noticed when both inputs IN_1 and IN_2 are connected and if we remove IN_1 (USB) our device gets reset.

VCC_USB = 5V

VCC_BAT = 6V

  • Hi, 

    Nshah said:

    We noticed when both inputs IN_1 and IN_2 are connected and if we remove IN_1 (USB) our device gets reset.

    VCC_USB = 5V

    VCC_BAT = 6V

    What do you mean by "reset"? According to your configuration, IN1 voltage (VCC_USB) drops below ~2.14V, the device will automatically switch to IN2( VCC_ BAT).

    Could you provide scope shots which describe the behavior you are seeing?

    Best

    Dimitri