This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Power muxes part recommendation request.

Other Parts Discussed in Thread: TPS25947, TPS2121, TPS2120

Hi, TI expert.

The customer requested Power muxes that meet the following conditions to apply to a new project.

- Input1: 5V

- Input2: 3.7V or 4.2V Battery(Li-Ion or Li-Polymer)

- Output Current: 4A ~ 5A

- Other: Notification of the power status currently in use

If there is a suitable product, please recommend it.

  • Hi Lee,

    Thanks for reaching out!

    Please look at TPS25947 (Figure 9-6 in the datasheet) 

    Best Regards, Rakesh

  • Hi, Rakesh

    Thanks for the answer.

    However, TPS25947 needs to be applied with two to apply with the above specifications.

    We request a recommendation again as a product that can be designed using only one part.

    Answers I'll wait.

  • Hi Lee,

    we have TPS2121 and TPS2120 but those cannot support continuous 5A. Please go through the datasheet and let us know

    Best Regards, Rakesh

  • Hi, Rakesh

    When I contacted the customer again, they said that it is okay to have an output current of 4A or more.

    Instead, we requested a recommendation as a product with an output ON/OFF function.

    ---------------------------------------------------------------------------------------------------------------------

    - Input1: 5V

    - Input2: 3.7V or 4.2V Battery(Li-Ion or Li-Polymer)

    - Output Current: 4A ~ 5A

    - Other: Notification of the power status currently in use (Device with ON/OFF function.)

    ---------------------------------------------------------------------------------------------------------------------

    If there is a suitable product, please recommend it.

  • Hi Lee,

    TPS2121 does it through ST and SEL pins

    Best Regards, Rakesh