Other Parts Discussed in Thread: STRIKE, CSD19533Q5A, CSD16301Q2
Hello!
Regarding the TPS2663 I think that the DRV pin is under-specified.
The datasheet specifies the following Electrical Characteristics:
Further down it lists the BSS138 as the MOSFET to choose.
From the datasheet of the Diodes BSS138:
This seems to fit.
The design guide TIDUED0 of the reference design TIDA-010009 states:
|
2.3.2.6 Selecting Q1, Q2 and TVS Clamp for Surge Protection |
The datasheet of the MOSFET CSD16301Q2 nonetheless specifies:
The BSS138 is usually not specified for 3V logic level, but the CSD16301Q2 is.
Now I do want to know more about the DRV pins characteristic, what is its driving characterstics?
Can it drive the CSD16301Q2, but what are the pros and cons, when using this MOSFET?
Is it slower in shutting down the main reverse polarity MOSFET because of the much higher input capacitance?
Or will it nonetheless discharge the gate of the other MOSFET in less time because of its much lower and specified RDS(on) for 3V logic-level driving?
Looking forward to answers from the TI gurus.