Hi, Ti member
I want to operate 100kHz and the maximum duty close to 99% by UCC25705.
have some questions about PWM IC design:
.
- the block diagram shows : this mode 0 , the timing of capacitor is discharge through low impedance directly to ground. (Is impendence 80 ohm?)
the timing of turn-off is the same at different Vff? (close to 75ns)
- what is limitation for discharge current of timing capacitor ?
- Can the UCC25705 operate at 1% PWM to limit power delivery ? the customer need soft-start and output current limit function (larger current but small voltage
thank you