hi everyone,
I see that the RC pin connection suggestion is contradicting with the Absolute Maximum Voltage Rating of RC pin itself.
Could someone please clarify this?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi everyone,
I see that the RC pin connection suggestion is contradicting with the Absolute Maximum Voltage Rating of RC pin itself.
Could someone please clarify this?
Hello Wilson,
The connection of the resistor from VIN to RC is correct. It might be misleading that the abs max rating on this pin is 10V, but the device charges and discharges the cap, so during normal operation it will not see a higher voltage.
hi Brigitte,
Welcome back from Thanksgiving.
Thanks for the explanation.
Having said that, at slowest frequency, the device should not charge the capacitor too long such that the final capacitor voltage reaches 10V and above.
Looks risky to me, if a user connect RC with small resistance and small capacitance value.