Other Parts Discussed in Thread: TPS61288,
Hi, TI expert.
Customers are looking for DC-DC Boost Converter to develop products with the following specifications.
If you search through the product serch under the conditions below, only one 'TPS61288' is searched, but 'TPS61288' is still under development, so the customer does not want it.
We ask if it is okay to use the TPS61022.
Please answer fast.
--------------------------------------------------------------------
[Specification]
- Input : 2.5V ~ 5V
- Output : 5V , 4A or more
--------------------------------------------------------------------