Part Number: LM76003-Q1
Other Parts Discussed in Thread: LM76002-Q1, , LM5576
May I know does the Does the LM76003-Q1 and LM76002-Q1 pass ISO7637 test? Could you share the test report?
We would design in dashcam application. The input voltage may have 12V and 24V, with the 5VDC@2A output. The Aux Camera Module shall not sustain damage when exposed to continuous voltages of less than 40V and load dump voltages of less than 75V as specified in ISO7637.
I also want to know the LM76003-Q1 is a good solution for this application. Or you have any good recommend.
BR,
Gary