Other Parts Discussed in Thread: LMZM23600,
Hi team,
Is it possible to directly replace LMZM23601 with LMZM23600 depends on load current, with adjustable output voltage?
One of my customers is considering LMZM23601 but the load current may (or may not) be smaller than 0.5 A, so they asked above question.
LMZM23600 and LMZM23601 seems to be pin-to-pin comparable. So I just wanted to make it sure that the direct replacement would be fine with adjustable output voltage without changing other component of the board.
Best regards,
Kurumi Hasegawa