Part Number: BQ76920
Other Parts Discussed in Thread: BQ77915, BQ78350-R1, BQ78350, BQ2947, BQ7718, BQ7716, BQ77908A, BQ76200
Hi Team,
I am looking for a 12V BMS(3*4.2V=12.6V) for a Li-ion battery pack.
Hence I came across BQ77915. It is stand alone.
But since we cannot store the Li-ion battery for a long time being fully charged, we are looking for another solution for the same and thus got the chip
BQ76920 with I2C interface.
After reading the datasheet, I've some doubts and I hope TI can help me with it.
1) External cell balancing is not recommended for this chip. But I believe it will be very helpful in my application. Would someone be able to help me with a reference design with external FET for balancing for a 3 cell battery pack?. Or can I just follow the design procedure in fig 9.3 on page number 22 of the datasheet of BQ77915 and also considering table 24 on page 41 of the BQ76920s datasheet.
2) Output current at REGOUT pin.
3) As per the table of recommended operating conditions the maximum voltage across a cell {VCn-V(Cn-1)} is 5V but my battery voltage is 4.2V maximum. Can I program this voltage through I2C?.
4) What is the need for BQ78350DBT IC?. or can I use any other controller to control the BQ76920 chip through I2C?. Can you suggest to me?.
5) I believe I can use the pin of the controller instead of the push button.
6) Is the controller connected to the REGOUT pin is power during the ship mode?.
7) I'm planning to use BQ24610RGER as the charger IC, I hope there won't be any problem with this.