This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7480-Q1: parallel battery packs with priority

Part Number: LM7480-Q1

Hi, I hope you are doing well.
I wanted to design a circuit to select a battery pack between three packs. batteries nominal voltage is 48V and there are two main packs and an auxiliary pack for failure situations. by powering on the system one of the main packs should be used until its voltage drops to 40V and then the second main pack should be inserted into the circuit. Also, the auxiliary pack should be ready to be switched on if any problem occurred for the main packs. So, I need a prioritized ideal diode for achieving the mentioned specification. I wonder if you could guide me to select a suitable component in this regard.

nominal Voltage:48V(max 54.6)

continuous load current: 10a

Max current 30A

Best