Other Parts Discussed in Thread: TPS2663
The evaluation board is rated for surge protection up to 500V (IEC610000-4-5 Level 1). I was hoping to modify it to handle up to 4kV (IEC610000-4-5 Level 4).
I have an operating voltage of 24V and a current up to 500mA. I tweaked the UVP and OVP setpoints and that seems okay.
But for modifying the surge protection level I tried removing the TVS and using the MOV V10E20P which has a current surge rating of 2kA which I need. However, when I tried running a surge test at +1.5kV it looks like the TPS2663 died on me and now all of the pins on it are shorting together. The clamping voltage of the V10E20P is 65V, is that a little too close to comfort for the maximum IN_SYS rating on the TPS2663 of 67V? Are there any recommendations on how to modify the front of the circuit to handle a surge of this size? The combination of EFT, overcurrent protection and reverse polarity protection are why I'm interested in the efuse.
Thanks,
Colin