We have questions about the circuitry for SDA and SCKL. From bq27545-Q1 EVM, it uses 100ohm for R6/7/8/9. Due to the system design, pull high resistance is low at system side, we worry about 100ohm may not able to pull data/CLK to low. Therefore, we would like to change 100ohm resistor to 49ohm for R6/7/8/9. Will there be any concern? Will it affect the ESD if using 49ohm instead 100ohm resistor? Thanks.