This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2051C: About resistance between OUT pin and GND pin

Part Number: TPS2051C

Dear experts,we use TPS2051C to design a charging protection circuit,we use a multimeter(FLUKE,179) to measure the resistance between its OUT pin and GND pin,and find that the resistance will be different. Most IC resistance values are displayed OL (the multimeter range is 0~60MΩ),it means they are greater than 60MΩ,but there are a few ICs with a resistance value of 30MΩ~50MΩ,is this difference in resistance normal?

What is the correct resistance between OUT pin and GND pin?

I appreciate your great help in advance.

Best regards,

Kevin