Other Parts Discussed in Thread: LM25180, LM5180
Hi Team,
My customer selected LM25183 for 5W DC-DC to dc converter for a gate driver power supply application, specification as given below.
Isolated DC-DC flyback converter
Vin : 22 - 26 V DC
Vout : 20VDC
Io : 250mA
Po : 5W
The webench design shows peak current for this design is 1A for 9.3uH primary inductance and 350kHz switching frequency. But on calculations getting around 3.25A peak for the same. Can customer directly go with webench design and use specified transformer (749196331).
Please help with your inputs.
Regards, Shinu Mathew.