Other Parts Discussed in Thread: TPS65982,
Hello guys. Thanx in advance for your attention.
I'm developing a dock-station device. TPS65982 and BQ25713 are used in the project.
I never adjust (via I2C comminication) BQ25713 ChargeOption0 register's PWM_FREQ field. As described in:
SLUSD83A – JUNE 2018 – REVISED JULY 2018:
PWM_FREQ: Reset state: 1b, that is equal 1b: 800 kHz <default at POR>
But in some cases I see the value is 1200KHz that is proved with an oscilloscope.
The SW mistakes (like bitwise shifting ones have been excluded).
I can't realize why PWM_FREQ field could start set as not <default at POR>. Like a workaround I always init PWM_FREQ as 1b at start.
But the issue is still making me concerned.
What reasons could be?