To whom it may concern:
We have a battery for power tools, which can discharge at high current, 15A to 25A. After several cycles, some of the batteries can't be used because the SOH was report below 60%.
After checking the fuel gauge, the FCC was only half of the design capacity, so the SOH was low.
A full charge/discharge cycle was applied with power supply and electronics load, and after this the battery recovered the FCC to over 95% of the design capacity, and SOH recovered as well.
2 batteries out of 150 had this problem so far. Could you help to do some diagnostic and find the solution?
Thanks a lot!
Chen