Other Parts Discussed in Thread: TPS92200
Hi support team,
Can the LM3402 use the following LEDs in 2 series and 9 parallel?
It drives 18 in total.
- LM3402 Vin: 8 ~ 36.5V
- LM3402 Dimming signal: Duty 0~100%, 190Hz±20%, 7V or less
- LED IF: 55mA
- LED VF: 2.85V
LED: NICHIA, NFSW757GT-V3
www.nichia.co.jp/.../NFSW757GT-V3-E(5466)Rs030.pdf
Regards,
Dice-K