This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61222: DCDC with the latch protection at short circuit

Part Number: TPS61222
Other Parts Discussed in Thread: TPS54J060

Hi, Team,

Now my customer is searching buck DCDC part with the latch protection at overcurrent(Vo shorted to GND).

The spec requested of IC is;

VIN range= max 6V,  Programmable VO= 2.4 ~ 3.3V , Iomax=50mA

Do you have any recommended part?

Regards,

H,Someno