Hi team,
The operating temperature range of TPS53317A shown on the webpage is -40~125℃, but in the datasheet is -40~85℃,which is the ture operating temperature range?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Reagan,
Sorry for the confusion. 85C is the maximum ambient temperature, 125C is max junction temperature.
Regards,
Ray