This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7H1101A-SP: Can board designed for TPS7H1101-SP with SS used for Enable to used with the newer A device

Part Number: TPS7H1101A-SP
Other Parts Discussed in Thread: TPS7H1101-SP,

Hi Experts!

My customer has a board designed to use the TPS7H1101-SP, with SS pin utilized for the enable function as well as soft-start. They have the collector of a 2N2222A transistor connected to pull SS low (emitter is at GND) to disable the device.

They would like to use the newer TPS7H1101A-SP on this same board.

Is there any performance or reliability issue using the SS pin on the TPS7H1101A-SP as a shutdown function instead of using the EN pin.

Best regards,

Jim B