Other Parts Discussed in Thread: BQSTUDIO
Hi,
One of my customers are experience issue with waking up from Autoship mode on some of their packs.
29th of November:
After further investigation of the TI eval board, I have discovered it won’t wake up with a load connected. When I removed the small load I had, see photo, the TI eval would wake up. This is because the small load dragged-down PACK+ enough to prevent a voltage greater than the wakeup voltage threshold to be presented to the gauge when pressing the Wake button.
Therefore, the TI eval board has not exhibited the fail-to-wake fault reported on 27th November.
I still have 5 batteries that do have the fail-to-wake though.
I am now going to perform a power cycle reset on these 5 and configure them not have auto shut down enabled and then periodically check them for correct behaviour.
27th of November:
Since the saga of the batteries failing to wake up, I have built up as many batteries as possible. I now have 26 batteries, most of which I have deliberately left untouched for the best part of two weeks.
This morning (27 Nov 2020) I performed a wake up check on the 26 battery packs. One of these 26 had the TI eval board mounted to the side of the 4S7P pack.
Out of the 26 battery packs, 6 of the packs would not wake up.
Six failures out of twenty six batteries is 23% and is broadly in line with the failure rate we discussed in the video call with a smaller total number of batteries. Of these 26, four were configured not to have AutoShip enabled. None of these four are in the failed state. If we exclude these four, the failure rate rises to 6 out of 22 which is 27%.
Obviously this is a completely unacceptable failure rate and it is urgent that the cause needs to be identified.
One of these six packs was the battery that exhibited the same behaviour in the email below. One of these six was the TI eval board (I showed this in the video call). I must say that I was surprised the TI eval board pack failed but ironically I feel somewhat relieved it did. The TI eval board does not have any additional circuitry and thus it is fair to conclude that the additional circuitry on the Blueprint BMS boards cannot be the culprit.
If we conjecture that the fault occurs only on batteries that have moved into the SHUTDOWN state and consider that at least one battery has failed to wake up on three occasions (the bad battery discussed in the email below), then perhaps we can form a hypothesis that the cause is a combination of the gauge’s silicon and the firmware when progressing to or from the SHUTDOWN state. Do you agree? If so, can you instigate some tests of your own?
For information, the markings on the BQ40Z50 gauge chips are:
TI 751 TI 841 TI 988 TI 988 TI 988 TI 988
CDEZ AG7Q AEEY AEEY AEEY AEEY
The first of these is the chip fitted to the TI eval board.