This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC29002: Question about LS pin (pin #7)

Part Number: UCC29002

Hi,

Load share bus: Output of the load share bus driver amplifier.

Will I add ESD components to protect the LS pin?

Tim

  • Hi, Tim

    Below is the application comments of LS pin from datasheet, so you don't need add ESD components.

    The LS pin is already internally compensated and has an internal 15-kHz filter. Adding external capacitance, including stray capacitance, must be avoided to maintain stability.


    BR,

    Yunsheng