Hi Sir,
For this device UCC28180D,
1)Can you tell me the soft start time of the IC?
Soft Start is programmed by the capacitance on this VCOMP pin.
also the same pin is used to provide the v-compensation,
Is there any chances of Voltage loop compensation being fast/ slow due to capacitor presence at pin for the both application
3) IC can be operated at 50/60Hz, We are operating it at 50Hz +/-3% variation .
so when i have frequency variation THD also varies ?
and how it will follow the AC line, as it does not have AC line sensing?
Thanks for your verification.
Regards,