This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2576: Inductor selection

Part Number: LM2576

Hello team,

My customer is trying to pick up inductor for LM2576-ADJ.

Using the formula in the D/S, they substituted Min(V) and Max(V) for Vin and Vout respectively, and calculated out the min and max values.

However, it straddles the range of H150 and L100. Could you please advise which coil should be used?

The maximum load current on the x-axis is 2.0 A.

Please find the detail from the internal link here.

Regards,

Itoh