Other Parts Discussed in Thread: LMG1205, LMG1020, LMG1210, ISO6721
Hi,
I'm looking at a 3-phase 48V, 22A peak H-bridge and want to use an EPC2022 as the transistor. I know I can use a LMG1205 etc as the driver for a non-isolated design but I need the power transistors isolated from the control signals. I was considering using the UCC21220A as an isolated driver but was unsure whether the clamping voltage is too high for the EPC devices.
Can you please advise the best way to drive isolated discreet GaN FETs with low Vg breakdown of only 6V?
thanks
Garth