This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: Operation without cells

Part Number: BQ76952

Is it possible to use the BQ76952 in an application without battery cells?  I am interested in using it for the current sensing + FET driver outputs, on a 48V system, but without battery cells.  I'm wondering if this is possible, perhaps by using a resistive ladder to spoof the cell voltage inputs.