Other Parts Discussed in Thread: LM74700-Q1
Hi team,
This device support ISO 7637-2 pulse 5a and 5b ?
Our customer want to replace from MAX16126/7/8/9 to TI device.
best regards
teritama
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
This device support ISO 7637-2 pulse 5a and 5b ?
Our customer want to replace from MAX16126/7/8/9 to TI device.
best regards
teritama
Hi Rakesh,
Thank you for quickly reply.
There are 24V and 12V both system.
And they want ISO7637-2 pulse 2a, 2b, 3a, 3b and 4 support information in addition to 24V and 12V support information.
Do you have some data?
best regards
teritama
Hi teritama,
I have available attached test results for LM76202-Q1. For LM74700-Q1, we have given available data in the datasheet.
ISO test results.zipBest Regards, Rakesh
Thank you for test data.
I checked it.
Let me check one.
Is it correct to recognize that the pulse not in ISO test results.zip and not listed in LM74700-Q1's datasheet is not supported?
best regards,
teritama
Hi Teritama,
The worst case scenarios are tested and test waveforms are provided in the datasheet. We suggest customer to use EVM and run the tests at system level as per their end manufacturer requirements.
Best Regards,Rakesh