This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65131: Need recommend a device could output voltage up to positive 20V and negative 18V

Part Number: TPS65131

Hi expert,

My customer used LT8582, and I recommend him to use TPS65131 to replace it. From customer, he prefer a device could output voltage up to positive 20V and negative 18V. (TPS65131 could only output positive 15V and negative 15V). Could you recommend a suitable device? thanks!

  • Hello Jiandong,

    I searched through ti.com and unfortunately we do not have a split rail (+/- output rails) converter that can output 20V/-18V. TPS65131 is the highest voltage split rail converter that I am finding which has +/-15V.

    Kind Regards,

    Liaqat