Hello
I choose TPS613222A to generate 5V from an 3.7 V accu li-ion in the aim to supply an USB plug. I need to have the max current of this device used alone( without any external components except the compulsory inductance)
I can't see in the datasheet the value of the permanent current that can deliver this device.
I saw peak current (1.10 A at the top of the first page an d1.8A in the device comparison table page 3)) but without any mention of duration. Most of the time, when it's a peak current, it's writte the duration (for example 10ms) of this value.
I did an experiment for 4 hours with 400ma in the load successfully but can you confirm that 1A is possible
Thanks