This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3435: About specifications

Part Number: LM3435
Other Parts Discussed in Thread: LM3549, LM3535

Hello Team,

I am comparing the specifications of LM3435 and LM3549.
LM3549 has a minimum LED current limit of 100mA.
On the other hand, LM3435 has a description of 1.2mA under I1.5A, 001h condition, so can I think that this IC can control LED current lower than 10mA?
LM3549 data sheet states that the current rise and fall times are 50usec maximum, but the LM3435 does not.
From Figure 19, it looks faster than the LM3549, do you have any specs or data?
LM3535 has internal feedback, which we believe is because the LED cathode voltage does not rise unnecessarily. Could you please tell me the approximate cathode voltage?

Best regards,
Nakayama