This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24750: BQ Studio + EV2400 testing

Part Number: BQ24750
Other Parts Discussed in Thread: BQSTUDIO, EV2400

Hello Team,

Does the BQStudio support BQ24750 for code verification?

My customer urgently needs it to verify a few codes.

Is there Maybe another module or method to do so?

Is there P2P compatible device available from the list?

Thanks and many regards,

Needhu

  • Hi Needhu,

    The BQ24750 is not an I2C or SMBus controlled charger, so unfortunately, it is not compatible with BQStudio and the EV2400.

    By the way, the device address and the register map are what determine whether two different chargers can share the same BQStudio configuration file. The charger's pinout is irrelevant for this. Since the BQ24750 does not have registers that can be controlled via I2C or SMBus, the BQ24750 is not compatible with the BQStudio configuration file for any of our other chargers.

    Best regards,

    Angelo