Other Parts Discussed in Thread: TPS65131
hello,
I have two questions about the specifications of the TPS65130.
No1
There is MIN "Vin + 0.5V" in VPOS of 6.5 Electrical Characteristics.
For example, when Vin = 5V, can + 5V be output from VPOS?
No2
How can I make sure that the VNEG output is started before or at the same time as the VPOS output when the power is turned on?
best regards