This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ77905: Connecting battery's in Parallel

Part Number: BQ77905

Hi,

I want to design the battery Protection. So i planned to use the BQ77905 IC. My battery Pack is 4Cells in Parallel & 3 Cells is Series. I can connect a 3 cells in series with the BQ77905 but shall i connect with that battery's in parallel. If not How i can connect the 3 sets of battery in parallel. 

Battery pack Spec:TI BMS.pdf

Nominal voltage 14.40V

Nominal capacity 6.90Ah

Initial impedance 200mΩ @ 1kHz at 20°C Max.

Charge current 4.83A Max.

Charge voltage 16.80V

Max. discharge current 10.00A

Peak discharge current 20.00A

Kind Regards,

Nishanth M